Other Parts Discussed in Thread: TPS25762DQ1EVM
Tool/software:
What are the conditions for the SINK_EN pin to transition to the active low state?
I'm observing SINK_EN and PPHV pin behavior on the TPS25730EVM. The EVM is configured for 9V minimum voltage (ADCIN1 decoded value = 1) and 9V maximum voltage (ADCIN2 decoded value = 1).
When I connect a USB PD source capable of 9V, I see PPHV rise to 5 V (vSafe5V), then SINK_EN transitions from high to low, then PPHV transitions from 5 V to 9 V.
If SINK_EN is intended to enable a downstream load, shouldn't this signal transition to active low after the PS_RDY message has been received from the PD source? The PS_RDY signal wouldn't be sent until the source has reached the agreed voltage in the PD contract.
Ch 2: PPHV
Ch 3: SINK_EN
My PD source is the TPS25762DQ1EVM.