This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ14203H: LMZ14203H_5_28

Part Number: LMZ14203H

Tool/software:

       

Dear TI Technical Support
 Question:
    We have decided to use the LMZ14203H and are designing a circuit.
     The specifications are as follows.
     Input voltage: 14V
     Output voltage: 12V
     Output current: 0.5 to 2.0 A
Ripple voltage: 50 mV or less
    The datasheet did not mention the potential difference between input voltage and output voltage.
     The datasheet did not describe the potential difference between the input voltage and output voltage.
     Is it possible to design with the above specifications of 14V input voltage and 12V output voltage?

                                                                                            Sincerely,

                                                                                                               yasuyuki  kumomura