Tool/software:
HI TI Team
1. Can the Power Path switch automatically without I2C control?
2. If the input switch needs to use the battery to power the input end when it is started, and then the input power is supplied to the system end, is this method possible?
3. Can the CC current be adjusted through software? For example: Is the CC current adjustable in steps of 1A, 2A, and 3A? If so, how should it be controlled?