Part Number: UC1845A
Other Parts Discussed in Thread: UC1845
Tool/software:
Hello,
The datasheet Figure 6-5 shows Maximum Duty Cycle vs Timing Resistance. It shows the maximum duty cycle varies 20% to 100% depending Rt values. However, the maximum duty cycle of UC1845A is 50%. So this means that Rt must be from 0.5Kohms to around 0.9Kohms at UC1845A?
Best regards,
K.Hirano