Tool/software:
Hello Team,
I was going through the datasheet for LM5163, but unlike the typical application where Vout =12v, I am planning on using it for an output of 5V. So in that case what could be the maximum current that I can draw from it given that my input voltage, Vin(min) = 40V, Vin(max) = 58, Vin(typ) = 51.2.
For my application I would be needing about 0.4A at max, normal mode of operation would be about 0.17-0.2A.
Thank you,
G Karthik.