Tool/software:
Hi team.
I have several questions regarding PMBus specification. TPS53667 is daisy-chained with PMBus and I2C in my customer's usecase.
1. is it possible to do daisy chain with PMBus and I2C on same bus(data line and clock line)?
2. I2C may operate at a clock frequency of 10kHz, so my customer would like to confirm whether PMBus of tps53667 works with a clock frequency of 10kHz. PMBus specification attached on this thread states that it can support a clock frequency from 10kHz, so we believe that TPS53667 can support the same.
3. If not, what is the minimum clock frequency of PMBus that TPS53667 uses to communicate?
Best regards,
Shunsuke Yamamoto