This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD18532KCS: The drain pin and the case are not internally connected. Is my understanding correct?

Part Number: CSD18532KCS


Tool/software:

Hi team,

The drain pin and the case of CSD18532KCS and CSD15842KCS are not connected internally. Is my understanding correct?

Best regards,

Shunsuke Yamamoto

  • Hello Yamamoto-san,

    Thanks for the inquiry. The drain pin (2) for a TI FET in TO-220 package is electrically connected internally to the metal tab. Please let me know if you have any additional questions.

    Best Regards,

    John Wallace

    TI FET Applications

  • Hi John-san,

    Thank you for the clear answer! It helps me to answer the customer's question. I apologize for the additional question after pushing solved button. My customer is looking for the FET which package is similar to TO-220 package and doesn't electrically connected drain pin and the package internally. Are there any TI's FETs which meet these requirements?

    Best regards,

    Shunsuke Yamamoto

  • Hello Yamamoto-san,

    Thanks for the update. We do not make any FETs in TO-220 or other packages with the drain pin not connected internally. These devices are constructed with the FET die sitting on the die paddle or tab of the package which is electrically connected to the center pin. In the D2PAK package, the center pin is trimmed and does not get soldered onto the PCB. The drain connection is made to the tab of the package. Let me know if you have any additional questions.

    Best Regards,

    John