This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28180: Gate Pin shorted at startup

Part Number: UCC28180


Tool/software:

Dear team,

I go through the Unknow gate failure issue. I checked on oscilloscope i found that my gate to controller ground pin i found that the voltage gone to negative but that is approx. 100ns and the voltage level is also vary from -100mV to -1.25V. So, my question is what the minimum time should be should it bear. and suggest also Schottky diode for that.

Thanks, and regards

  • Hi Munna,

    It would be best to determine the root cause of why the gate is going negative. Violating the -0.3V abs max rating can instantly damage the pin. A Schottky diode might help, but you may have a layout issue.

    I hope this helps.