This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP38692-ADJ: VIH and VIL values for EN pin

Part Number: LP38692-ADJ

Tool/software:

Please provide all the minimum and maximum values missing in the above image (Marked in red box).

  • Hi Kartihk,

    The min and max values in the electrical characteristics table are chip specifications, guarantees we make within recommended operating conditions. Therefore, I am unable to provide min and max values that aren't in the datasheet because that would require redefining the product. Since there's no minimum where a low voltage stops being off without violating abs max we didn't specify a min. Likewise, since there's no point where an ON voltage is too large to be ON without violating abs max we did not specify one. 

    On a practical level, defaulting to the abs. max limits (min -0.3V and max 12V) may give you a number conceptually similar to what you're looking for.

    Best,

    Gregory Thompson