This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS630250: Ti Webench Design Query

Part Number: TPS630250
Other Parts Discussed in Thread: TPS63802, TPS631000

Tool/software:

Hi TI Team,

I am looking to use a Buck Boost converter for one of our projects. The specs are Vin = 3V - 4.2V and Vout = 3.3V @ Iout max = 1.5A.

I searched on TI Webench and came across a base part number TPS630250 which fits best as per my requirement.

However, we do not want to use the BGA package and want to use the QFN package of the same base part number. But the QFN package part number is not shown in the TI Webench.

So, can I use the BGA package' Webench design and just replace the BGA package with QFN package keeping the rest of the design same?

Your quick response will be highly appreciated.

Thanks & Regards,
Sahil Nayak