Tool/software:
Hello,
I have a question regarding the turn ratio (TR pin) configuration. What is the use of this pin if we are already using one opto to feedback voltage? Lets say the transformer has turn ratio of 4 or a turn ratio of 10... how to setup this pin?
Maybe related question: There is a peak current limit (IPK pin) but no average current limit, right? If so, the output current limit need to be implemented by turning on the opto with a custom circuit placed on the secondary side, right?
Note: In our design, we don't need the full power of the chip (20W is enough), but has interest in the 500KHz capability.
Thank you,