This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: How to set GE pin when using a level shifter that requires pull ups

Part Number: BQ35100

Tool/software:

Hi,

I'm using the BQ35100 with the LSF0204RUTR level shifter.  The processor operates at 1.8V while the BQ35100 is being operated at VBAT which is 3.6V.  When the GE pin isn't being drive high it is pulled low via a 1M resistor has shown in the reference design.  Currently, when the GE pin is set high by the processor, the level shifter only outputs 1.8V to the GE pin.  I believe the input to the GE pin needs to be higher than 2.65V to enable.  In order to bring that pin up to VBAT it would need a pull up resistor to VBAT, however, when switched off I don't believe it would be able to go low.  What is the best way to interface the GE pin with the level shifter to ensure operation and minimal current draw when off?  See attached image for the schematic.  Please let me know if you need any additional details.