Other Parts Discussed in Thread: UCC5350
Tool/software:
Hi,
Could you list out the pros and cons of the MC and SB version and how to choose a version?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi,
Could you list out the pros and cons of the MC and SB version and how to choose a version?
Hi Zehui,
The split output version lets you to use a different turn-off resistor and turn-on resistor without needing an extra diode and its associated diode drop. This can be used to fine-tune the efficiency vs. overshoot of the FET switching. However, any Miller injection current will have to drain into the turn-off resistance. A turn-off resistor >0 will directly increase the Vgs Miller spike voltage.
The Miller clamp pin will provide 0 ohms of impedance to the Miller injection current, resulting in the lowest possible Vgs Miller spike. It is an additional FET in parallel to the main pull-down NMOS, so it provides lower Miller impedance and stronger turn-off when combined with a 0 ohm turn-off.
I usually recommend optimizing the HV bus to eliminate switch node ringing, not increasing Rg and switching losses. Therefore, I recommend the Miller clamp version, with a minimal Rg (1-5 ohms). The UCC5350 already has an asymmetric internal Roh (12 ohms) and Rol (0.5 ohms), and this is sufficient to limit ringing in a well dampened and decoupled half bridge. It may just require adding more high-voltage decoupling and snubbing.
Best regards,
Sean
Hi Sean,
Thanks ror reply!
Is there a more intuitive selection recommendation, such as at what bus voltage level a Miller clamp becomes necessary?
Hi Zehui,
If you are using a SiC FET or IGBT, which are are more suitable for a Higher BUS voltage, the split output will probably be sufficient. If you use Si FETs, you will likely require the Miller Clamp.
Best regards,
Sean