This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22992: TPS22992

Part Number: TPS22992
Other Parts Discussed in Thread: TPS25947

Tool/software:

Hi Team,

1.We are working on a project , which is using USB Type C, sink  mode, 5V,3A design. The capacitor value is greater than 200uF because of circuit limitations. In the USB4 certification test our board failed in the below inrush case
From 0-100ms, any current exceeding 100mA shall have a charge less than 50uC
- From 100ms-1s, there shall be no current exceeding 100mA.
Since the product is in production phase and also very small form factor we are unable to use the dedicated USB PD controller. Can you suggest some suitable inrush current limit switch for VBUS path from TI overcome the issue?
2.For the same case we are planning to use the device TPS22992SRXN.In the datasheet the capacitance value for CT pin is given upto 4700pF for 5V Vin, Can you please confirm is there any maximum capacitance value restrictions that can be connected to CT pin? Since we need 1S delayed Vout, CT needs to be a higher value.
Early response will be appreciated.
Thanks,
Vidhya
  • Hello Vidgya,

    Welcome to E2E.

    1. TPS22992 VIN range is 5.5V. Do you need more margin for 5V USB application? For most USB application reverse current blocking and reverse polarity also required.

    I can suggest TPS25947 for up to 20V PD application and TPS2521x for 5V PD application.

    2. We don't have max cap restriction on CT cap. You can evaluate the slew rate you want and use appropriate CT or dVdT value.

    Thanks 

    Amrit