Other Parts Discussed in Thread: UCC28950,
Tool/software:
Hi , can i operate the UCC28950 as a bus converter ? what should i change in the application to operate the UCC28950 with no feedback ?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi , can i operate the UCC28950 as a bus converter ? what should i change in the application to operate the UCC28950 with no feedback ?
Thank you
Hello Alon,
Yes, you can operate the UCC28950 as a bus converter if you wish.
You simply have to fix the PWM duty cycle to a constant value that delivers the output voltage based on the input voltage and transformer turns-ratio.
Depending on the input and output specifications, the UCC28950EVM-442 may or may not be able to meet your requirements without extensive modification.
Fixing the duty cycle means keeping the COMP output at a constant voltage.
Since the EVM loop compensation is an integrating one, you can't simply tie the VSENSE input network to VREF.
I suggest to remove the integrating caps from COMP and give it a resistive load. Then you can set the VSENSE divider on the EA- input appropriately to achieve the error voltage needed on COMP for the duty cycle needed for your application.
Regards,
Ulrich
Hello,
Max duty cycle for this device is 95% typical with a maximum duty cycle of 97%. Even though it is not specified the minimum maximum duty cycle is 93%. That being said if you want to run at maximum duty cycle. That being said if you want the controller to always run at maximum duty cycle I would tie the EA- pin to the comp pin setting up the voltage amplifier into a voltage follower. Then set the EA + to 3 V with a resistor divider off of VREF.
Regards,