This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLVM23615: Electrolytic input capacitor for TLVM23615 and 100m cable

Part Number: TLVM23615

Tool/software:

Hello,

I'm evaluating TLVM23615 for the following application:

Input voltage: 7.4-30V (with UVLO)

Output voltage: 5V

Maximum output current: 150mA

Input cable: 100m shielded twisted AWG26

Conductor DCR: <150 ohm/km

Capacitance: 85pF/m @1kHz

Ground capacitance: 150pF/m @1kHz

Characteristic impedance: 75 ohm @1MHz

According to section 8.4 (Power Supply Recommendations) of the datasheet, is an electrolytic input capacitor mandatory/suggested for this application?