Tool/software:
Hi,
We would really appreciate it if you could answer these questions related to the design for the support of TPS546E25.
- At J9.11, SW the output terminal has the filter connection in the simplified Schematic. Need to confirm if this pin can be connected to ground via a 1.0k resistor would suffice.
- Also, capacitor requirements at the J9.20 PVIN. (Input voltage)( Typical Application in the data sheet shows 100uF x 3, 22uF x 8 and 0.1uF x 2 ) . Do we need these many caps? How many are required at minimum?
Thanks!