Tool/software:
Hi all,.
We are considering using this FET as an alternative to the Renesas HAT2114RJ.
[Conditions]
After the FET is turned on, a reverse electromotive voltage is generated for 17 μs.
When ON, the current is 3.3 A peak.
Vdss due to the reverse electromotive voltage is about 74 V.
Continuously, it continues about 120 times at the maximum.
Renesas HAT2114 has a continuous pulse avalanche rating but I understand TI's avalanche rating is one time.
Is it possible to guarantee the above use cases? Or could you give us some comments? such as if the avalanche energy is in the specifications and there is no problem.
I would appriciate if give me any advice.
Best Regards,
Ryusuke