Tool/software:
Hello,
According to the datasheet of LP87524J-Q1, the following output capacitors are recommended.
However, we are planning to use different capacitors for our application.
We would like to get your confirmation on whether our selected capacitors are acceptable.

We would appreciate your feedback on the two inquiries below:
-
We are considering using Taiyo Yuden MCASJ31LAB7226KTNA01 as an alternative to the recommended output capacitors. The main differences appear to be the rated voltage and ESR, but given our output voltage level, we do not expect any issues with the rated voltage. Could you please confirm if this capacitor is acceptable or if there are any potential concerns?
-
For a 3.3V output rail with a maximum load current of 50mA, we are planning to use a 10uF output capacitor instead of 22uF. Due to the low current, we believe this should be sufficient. Could you please confirm whether this is acceptable?
Thank you in advance for your support.