Part Number: UCC27201A
Other Parts Discussed in Thread: UCC27201, CSD18563Q5A,
Tool/software:
Dear Texas Instruments Support Team,
I hope this message finds you well.
I am currently using the UCC27201 high-side/low-side driver in a power switching application, supplied with 12V. The driver operates as expected when there is no load or when connected to a high-resistance load. However, I encounter a critical issue when connecting a low-resistance load: the driver begins to heat up significantly and eventually gets damaged.
The MOSFET used in the design is the CSD18563Q5A, and the configuration follows standard recommendations as per the datasheet. I have ensured proper decoupling and layout practices. The issue seems to arise specifically under higher load conditions.
I would like to understand the possible causes of this problem. Could it be related to shoot-through, incorrect dead time, excessive switching losses, or gate driving issues? I would appreciate it if you could help me identify the root cause and suggest any modifications or protections I can implement.
If needed, I can provide schematic diagrams and scope captures of the switching behavior.
Thank you in advance for your assistance.
Best regards,