Tool/software:
Hello,
I'm doing SCH and PCB for the TPS631010YBGR part and I'm a bit confused by the datasheet.
See images below.
Suppose I have an 0402 and 0805 on the input side and two (not three) capacitors on the output:
1) Which capacitor should the 0402 be, #1 or #2?
2) Since I only have two out equal capacitors, which can be omitted: #3 or #5?
Note: I am aware that I named the output rail 3.3V but used an 806kΩ. Please disregard this peculiarity.