Other Parts Discussed in Thread: UC2854, UC2854A
Tool/software:
We would like to understand the current limiting mechanism of the UC2854B PFC controller.
In our design:
- The multiplier block receives inputs from:
- The DC output voltage through a resistor divider connected to the VSENSE pin.
- The DC input voltage through a resistor divider connected to the IAC and VRMS pins.
- Current sensing is implemented using a 2 mΩ shunt resistor (Rsh) placed in series with the boost inductor. The voltage across this resistor is connected to the ISENSE pin to measure the instantaneous inductor current.
- This signal is processed through the current error amplifier, whose output is compared against the PWM ramp to control the duty cycle.
We are specifically interested in understanding:
- The function of the ISENSE pin in relation to the current control loop.
- The role of the PKLMT (Peak Limit) function in the UC2854.
- How this peak current limiting is implemented and how it behaves during normal operation and overcurrent conditions.
- How will the multiplier work.
Our application requires boosting the input voltage from a minimum of 50V up to 410V, and we would like to ensure that the current limiting mechanism is properly configured to protect the circuit and operate efficiently under varying input conditions.
Kindly explain how the ISENSE and PKLMT functionalities work in detail, specifically in the context of our setup.