This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2842: IS UC1842/2842/3842 can be use as open loop configuration

Part Number: UC2842
Other Parts Discussed in Thread: UC1842

Tool/software:

In my project, we require a SMPS with an input voltage range of 120V to 200V DC and an output voltage range of 30V to 50V DC. The application demands an open-loop configuration, meaning the output voltage is allowed to vary proportionally with the input voltage. I would like to confirm whether the UC1842/2842/3842 PWM controller ICs can be used in such an open-loop setup. Is any alternative part number better suited for this requirement.