This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92664-Q1: Individual LED Powr and intensity control

Part Number: TPS92664-Q1

Tool/software:

Hello Experts,

I'm relatively new to the automotive field and have a question. I want to drive 10 LEDs with independent on/off and intensity control. Each LED has a forward voltage of up to 3.5V and requires a current of 220mA.

From my understanding, the LEDs are connected in series, and the device is capable of controlling each LED independently. According to the datasheet, the maximum current is 1.5A. Therefore, if I'm correct, this LED Matrix Manager (LMM) will be set up as a constant current source of 220mA with individual LED control.

Does this meet my requirements?

Best regards,
Vishal Kakade