Tool/software:
Hi Team,
TPS544C20 Abnormal voltage rise waveform during startup


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
TPS544C20 Abnormal voltage rise waveform during startup


It a little hard to determine what is going on at 20ms/division, but I agree that it is not normal for the TPS544C20 to take 70ms to power up.
One clear error in the schematic is PR131. There should not be a connection between AGND and PGND external to the IC. This can significantly impact the accuracy of current sense and may be triggering over-current protection despite low current due to the introduction of a ground loop.
AGNDSNS is internally connected to PGND, and this should be the only connection between AGND and PGND.
Additionally, It looks like there is not enough output capacitance to stablize the D-CAP2 control loop with C690015 (470pF from DIFFO to FB) in the feedback.
I would recommend trying to remove PR131 and C690015
Hi Peter,
This issue has not been improved after modification
Are there any other methods?
Thanks
You removed both PR131 and C690015?
Are you able to talk to the part via PMBus? Knowing what status bits, if any, are being set would be very useful
Can we zooom into the start-up?
The soft-start time is suppose to be 2.7ms, so it would be good to look at the rise times to see if the part is starting up as intended, at about 1V/ms, or if it is being delayed some-how.
Can we include VIN/VDD with the start-up?
Zooming into the middle portion where the output is a saw-tooth at higher frequency would also be useful.