This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR33620: Alternative with an adjustable soft start time

Part Number: LMR33620
Other Parts Discussed in Thread: LMR14020-Q1

Tool/software:

Hi,

We use the LMR33620ADDA in several projects. For a new project I'm looking for a similar part but with an adjustable soft start time that can be configured down to 1ms.
If possible it should have a higher maximum input voltage (as e.g. LMR36520FADDA) as 36V is always a bit limiting for 24V input voltage.

Output voltage is 3.3V. Synchronous step down is mandatory.

A fully integrated power module (integrated inductor) is also possible.

Any suggestions are highly appreciated.

Thanks and best regards,

Patrick