Tool/software:
Hello,
I am working with the TPS25762 and would like to know if it is possible to configure the PDOs to support USB data communication over the USB Type-C port, alongside USB Power Delivery. Specifically, I am referring to the "USB Communication Capable" bit that can be set in the Source_Capabilities message.
Could you please clarify whether this feature is supported via GUI in the TPS25762?
Additionally, I am planning to work with the TPS25763 as well. Would it be possible to obtain the base firmware binary for the TPS25763?
Thank you in advance for your support.
Best regards,
Fabrizio