Tool/software:
hello,
I am using the TPS22811 as a switch in my circuit. I have a filtered 12V input to the IN(pin 5) of the chip. The EN_N/OVLO(pin 2) is the 12V input stepped down using a voltage divider(the voltage divider brings in the input down to 1.07V. The EN/UVLO(pin 2) is a 3.3V signal coming from a voltage sequencer chip(LTC2977). The DV/DT(pin 7) is connected to a 3300pF cap. The IMON(pin 9) is connected to a 1kΩ resistor that is tied to GND. The output has a 10uF cap on the output.
This circuit normally has a 5A load on it and behaves as normal. However I need to have short circuit protection for this chip and I observe two issues when I short the output to GND.
First issue: When I short the output to GND I observe 37A from the output to GND before the output shuts off due to short circuit protection. The datasheet says the output should latch off but after the short is removed after about ~6 seconds the output turns on even though I did not toggle the EN/UVLO pin off/on or cycle power. Why is output not latching off?
Second Issue: When I briefly apply a short I see the output shut off. However after the output has shutoff I toggle the EN/UVLO pin off then on again which should turn the output back on. However I observe that the output turns on ~2 seconds after the enable signal goes high. Its almost as if the unit is in some of reset mode after the short.
Any advice would be appreciated.
Thank you