Other Parts Discussed in Thread: LM51772
Tool/software:
I'm looking for a recommendation of a part we could use to charge a bank of ultra capacitors (~1200F at 15V) with a constant current. It will be used for either 12V or 24V systems. It would be great if one circuit could support both systems, but having different population options is acceptable. For the 12V system, it needs to charge the caps to 15V, so we need a buck/boost regulator. For the 24V system, the caps need to be charged to 30V. The charge current does not need to be precise, but nominally we want 20A charging for the 12V system and 10A charging for the 24V system. Please let me know if there is a part that would be well suited to this.