Other Parts Discussed in Thread: ISO7710
Tool/software:
Hello,
I am an FAE at a distributor that handles TI products.
I have received three questions from my customer about the operation of an active clamp flyback.
This question is the same as the following thread.
(Question 1)
I am experiencing a phenomenon where the mode switches back and forth between LPM and ABM, and between ABM and AAM.
I have attached the waveforms.
Even if the load is constant, the mode switches back and forth between LPM⇔ABM and ABM⇔AAM at the time of mode transition.
Are there any reasons why this might be happening?
Could you tell me if there is any way to improve it?
(Question 2)
A ringing current flows between low side turn-off and high side turn-on.
I have attached the waveforms.
The area indicated by the red frame.
It is unclear whether this is due to superimposed noise or the effect of the resonant current in the high-side loop.
(Question 3)
When ABM is on and Nsw is 3, the second Hi side gate signal is not output.
Waveforms are attached.
Since it has been confirmed that a signal is being output from the UCC28782 PWMH, it is assumed that this is due to the fact that no signal is being output from the ISO7710 out.
Changing the capacitor between VCC2 and GND2 of the ISO7710 has no effect.
Please let me know if there is any way to improve this.
Best regards,