Other Parts Discussed in Thread: BQSTUDIO
Tool/software:
We used BQ4050 for two string designs and found two problems in batch production. We have not been able to find the cause yet. Can you help us investigate
The product application is a two string battery with 4 indicator lights, and the configured charging wake-up current is about 300mA
Problem 1: During the first power on charging activation (charging current 2A), if the charger is turned off after activation, the light will still flash abnormally for about 20 seconds, which corresponds to the configured CC wake up time. The abnormality is 100% reproduced
Problem 2: After aging during assembly, if left idle for more than 10 hours, charging (charging current 2A) may occur, and the light may not turn on immediately. It takes about 20 seconds for the light to turn on. This time corresponds to the configured CC wake up time, which is abnormal with 5% recurrence
Can you please confirm the possible causes of the above issues? Please find attached the GG file for this project