This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25946: IEC62368

Part Number: TPS25946

Tool/software:

Hi All,


I have a question about IEC62368.

TPS25946 is IEC62368 certified.

If IEC62368 has been obtained for eFuse, can we say that the application in which it is installed has also been certified for IEC62368?

Or does the application itself need to be IEC62368 certified? I don't know the scope of IEC62368 certification, so please let me know.

If a customer is going to obtain IEC 62368 certification for their application, I would like to know the benefits of using an IEC 62368 certified device for eFuses such as the TPS25946.


Best Regards,
Ishiwata