Tool/software:
Hi sir whenever i connect c type usb of voltage 5v to Vbus i am facing issue in Regn pin ,Regn voltage is present for few seconds then it is not present so i replaced the capacitor of 4.7uf with 50 v rating immediately regn voltage is dropped from 0.5v to 0v followed by i checked the continuity resistance it is short with Gnd .Can u mention what are the possible reasons for this REGN pin failure ? Because initially after soldering the ic I checked the resistance between Regn pin and Gnd it is 493ohms only after giving supply to the ic iam facing this issue.
kindly give me possible reasons for this failure of regn pin