This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV761: TLV76133DCYR Qualification Grade, Minimum Load Current, Thermal Regulation and Temperature Stability

Part Number: TLV761

Tool/software:

Hello Team,

We are planning to use part TLV76133DCYR in our design.

I required below data:

1) Qualification Grade

2) Minimum Load Current

3) GND current

4) Thermal Regulation

5) Ripple Rejection

Thanks & Regards,

Jignesh Karena

  • Hey Jignesh, 

    Yes, please see answer below also pelase see datasheet all of this information can also be found there. TLV761 Datasheet

    1) This is industrial grade device. 

    2) The minimum load current 150mA 

    3) Quiescent current 100uA maximum 

    4) DCY (SOT-223) packge, R_theta_JA is 95.4 degrees C/W

    5) PSRR 70dB at 120Hz

    Hope this helps! 

    McKyla