This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3842: Recommendation for buck converter using external PNP transistor

Guru 12965 points
Part Number: UC3842
Other Parts Discussed in Thread: LM5148, LM25190, LM25149, TL494,

Tool/software:

Hi,

We are currently supporting a customer who is designing a non-isolated buck converter with the following conditions:

・Input voltage: 18V to 50V
・Output voltage: 15.2V to 16.8V (adjustable)
・Output current: 0.9A
・Inductor: 100µH (external)
・No transformer (non-isolated)
・High-side switch: external PNP bipolar transistor (2SA1577: https://fscdn.rohm.com/en/products/databook/datasheet/discrete/transistor/bipolar/2sa1577t106q-e.pdf)

The customer is considering using a PNP transistor as the high-side switch to simplify their driver stage, and they are seeking a suitable TI controller that can support this topology.

We have reviewed several synchronous buck controllers such as LM25149, LM5148, and LM25190. However, we understand that these devices utilize bootstrap-based high-side gate drivers designed for N-channel MOSFETs, making them unsuitable for directly driving a high-side PNP transistor (which requires a base voltage lower than VIN).

Given the use of a high-side PNP transistor, could you please advise:

1. Whether there is any TI controller that can support this type of configuration (i.e., directly driving a high-side PNP BJT in a buck topology)?

2. If not, do you have any recommended workaround or reference circuit using TI products that could enable PNP-based buck conversion under these conditions?

If any older analog controllers (such as UC384x family) or low-side PWM controllers are still applicable for this purpose, we would appreciate your guidance as well.

We look forward to your suggestions.

Best regards,
Conor