This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: CC Gain value

Part Number: BQ28Z610
Other Parts Discussed in Thread: BQSTUDIO

Tool/software:

During bring-up of our device we skipped the current calibration because the note on the technical reference says it's not necessary  due to "hardware improvements in this device" (and we're using a 1mR shunt as suggested).

During testing we found that the reported current was approximately 1/3 lower than actual current, and upon further investigation we've found that CC GAIN is set to 3.58422 which would explain that error.

Do we need to run gain calibration or should we just change CC GAIN value to "1"?