This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23755: creating a POE-powered pass through gateway

Part Number: TPS23755

Tool/software:

 We want to design a gateway which need to support 2x  RJ45 LAN port  

LAN1 plans to be as PoE port, when the data is daisy chained from LAN2 toLAN1, it would be very nice the data (Switch function LAN1 and LAN2), but also the PoE is Passthrough by LAN2, so that with the daisy chained (Loop thout/PassThough) ,2nd gateway  is also powered via 1st gateway's LAN2.

Could you provide suitable solution for this requirement?

Thank you !

  • Hi simon,

    Thanks for reaching out!

    I am wondering if below structure works for your case. It is for 25W (class-4) power case. 

    Could you let me know what is the power needed for the 1st RJ45, and what is the power needed for the 2nd RJ45.

    Best regards,

    Diang