Tool/software:
Hi team,
Can the following configurations be set in EEPROM?
- The set has two power inputs: DC IN and USB-C.
- When DC IN input is present, USB-C functions as a 5V/3A source (does not sink).
- When there is no DC IN input, USB-C functions as a 20V/3A sink (not a source).
- When sinking, the USB-C will not accept power from sources less than 20V/3A (power path remains closed)
Best Regards,
Ryu.