This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76972: Unexpected Wake from SHUTDOWN on BQ7697202 via TS2 Pin with high edge.

Part Number: BQ76972


Tool/software:

Hello TI team,

I’m working with the BQ7697202 and observing unexpected behavior related to SHUTDOWN wake-up via the TS2 pin. According to the BQ76972 Technical Reference Manual, the device should only wake from SHUTDOWN when:

  • TS2 is pulled low (below ~1.5 V),

  • A voltage is applied to LD, or

  • Any VCx pin exceeds ~1.2 V.

However, in my case:

  • I am applying a DC 60 V signal to the TS2 pin.

  • A TVS diode is used on TS2 to clamp this voltage below 6 V (within absolute max limits).

  • Despite this, the device exits SHUTDOWN and powers up — even though TS2 is not pulled low at any point.

  • This is a clean DC signal, not a transient — no falling edge is present.

This behavior seems to contradict the documented wake-up methods, and I want to understand:

  1. Is there any known internal mechanism that could explain this wake-up due to TVS clamp behavior?

  2. Could leakage or ESD clamp current on TS2 result in false wake-up detection?

  3. Are there any undocumented limitations or edge cases related to using TS2 with external clamping?

For completeness:

  • The BQ7697202 enters SHUTDOWN via the SHUTDOWN() subcommand.

  • There is no thermistor or pull-down on TS2.

  • REG18 is left unused.

  • TS2 is connected only to a TVS diode referenced to VSS, clamping at ~5.8 V.

I’d appreciate any insight into whether this is expected behavior or a potential risk of backfeeding or ESD leakage during system design.