This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM64406E: TPSM64406E

Part Number: TPSM64406E
Other Parts Discussed in Thread: TLVM14406

Tool/software:

Hello,

This is a call for DC/DC suggestions.

The crucial issue here is extremely low radiated and conducted emissions.

As for output ripple, we could always add an LDO if needed.

I see that both the TPSM64406E and TLVM14406 are described as ultra-low noise in the selection table.

Is there any real difference in their noise performance?

Would we achieve the same or better noise (radiated / conducted) in a non-module solution?

For an additional application where the input is 8-20V, output 4V and output current around 700mA, what would be the best lowest noise candidate?

Thanks in advance,

David

.