Tool/software:
Hello,
We are planning on using the BQ35100 IC in accumulator mode to monitor state of charge of a Li-SOCl2 battery. To save power, we will only periodically wake up the system for tens of milliseconds at a time. We want to be able to accumulate the coulomb counter for that small duration.
When I look at the datasheet, Table 6.11 specifies that the coulomb counter has a conversion time of 1 second. In section 7.3.2.1, it also says that the device measures and updates voltage, temp, and current every 1 second. Does this mean that the accumulator will not be able to sample fast enough to account for our tens of milliseconds long awake cycle?
When I read section 8.2.2.6, it explains that the device is designed to work in a system where there is a period discharge pulse of tens of mA for tens of milliseconds. This seems to contradict the two specifications above.
Any clarification would be much appreciated.
Thanks,
Gabe