This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM23600: Clarification Request on VIN Max Rating

Part Number: LMZM23600


Tool/software:

Hello

  • When we initially considered the part LMZM23600SILR, the datasheet (Rev B) specified a maximum input voltage of 42V. We have now noticed that in the updated datasheet (Rev C), this has been revised to 40V.
  • Could you please clarify the reason behind this change?
  • Was the earlier value of 42V a typo error in the previous revision of the datasheet ?

Or

  • Has the actual absolute maximum voltage rating for the part been reduced based on further validation ?