Other Parts Discussed in Thread: BQ51013C, TIDA-00318
Tool/software:
Hi
I am designing a wearable RFID reader, and as part of my application, I want to incorporate a wireless Qi2 compatible receiver that can charge a 1S1P battery at 4.2V. If TI has any Qi2 compliant chips with a suggested RX coil, that would be great to know. Otherwise, what other choices do I have? Given that the product is modest, measuring about 40 mm (w) by 60 mm (l) by 40 mm (h), the coil's size must be taken into account. Since the application is only in RX mode, any rating between 5W and 15W is adequate. Please give me any RX IC recommendations that I can utilise.
Kind Regards
DA