Other Parts Discussed in Thread: TPS25751
Tool/software:
Hello TI,
I'm working with a custom board with TPS25750 (will be replaced with a 25751 in the future) and the device fails to contract the power role when connected with a usb type-c port of a notebook.
The TPS is set with the following settings:
- power role Sink and Source
- preferred role SOURCE
- 15W Sink and Source
- No USB data
The scenarios are as follows:
- Connected to a phone, the tps is source and the phone is sink. OK
- Connected to a notebook, neither tps nor notebook becomes sink or source so nothing happens. FAIL. In this case the tps should be sink and the notebook should be source.
I tried the 4cc command SWSk to swap to sink while the tps is connected with the notebook but the command is rejected.
If I use a FW with preferred power role SINK the notebook works as a Source and the tps as a Sink and it's correct, but by default I have to start with preferred power role Source.
Do you have any suggestion? I attached the configuration file of tps.
conf_tps
Thanks in advance!