This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1H000-Q1: 10mA preload needed for FAULT?

Part Number: TPS1H000-Q1

Tool/software:

below was measured on the TI EVM  jumper as shown (red color on schematic image). (auto-retry mode)

Power on 25V and put add electronic load on output to GND.

The issue on FAULT signal Pin:

When Load = 0-4mA; Fault=0.

Load = 5-9mA; Fault signal is jitter.

Load is >=10mA; FAULT = 1.

Over load (set 3.24K is 200mA); FAULT=0.

Our understanding is that FAULT should be high when load is 0-10mA and less than the set current limit. 

Is there something wrong with the jumper/schematic setup?

Thanks for any comments on this!