Other Parts Discussed in Thread: BQ25856-Q1
Tool/software:
I see (from related question) that by shorting SYS to VAC, BQ25750 can supply power from battery to input (VAC). I also see (from documentation) that once the voltage at VAC is within the limits of ACUV/ACOV, the chip will return to forward operation. The reverse voltage I want to set up is within the limits of ACUV/ACOV. Will this cause the chip to immediately return to forward operation once the reverse voltage is set up at VAC?
Using BQ25856-Q1 this is not a problem, but I know these chips are different in that that BQ25750 is designed for direct power path control, while BQ25856-Q1 is not.
The reason I ask despite already having a chip doing what I want (BQ25856-Q1), is that I want, if possible, to define an alternative component for the BOM.