Tool/software:
I want to reduce the current that will be detected as an open-load for TPS1H000-Q1. At 6V min supply and max Iol,on of 8mA, a load of >750ohm will trigger an OL fault. This may result in false open-load triggers in my application. Is there a way to push this open-load detection to >2kohm (Iol,on of 3mA)? If not, is there an alternate device that could achieve this?
Thanks,
Matthew Guibord