This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Current shunt resistor value and SOC jump at rest

Part Number: BQ34Z100-R2

Tool/software:

Hello,

I’m currently working on a project that uses the BQ34Z100-R2 fuel gauge to monitor the state of charge of a 15S1P LiFePO₄ battery pack. I’ve successfully completed the learning cycle and generated the corresponding golden image file. However, I’m noticing SOC jumps of up to 10% while the system is at rest. The ChemID file was provided by the TI ChemID team.

The board is designed with a 1 mΩ shunt resistor for current measurement, and I’m beginning to suspect this may be related to the behavior I'm observing. I came across a forum post (TI E2E link) where it was mentioned that the minimum recommended shunt resistor value should be 5 mΩ. However, the reference design for the BQ34Z100-R2 uses a 1 mΩ resistor which seems to be contradicting the Technical Reference Manual.

Could you clarify what the minimum shunt resistor value should be for a system with a rest current of around 30 mA? Additionally, could the use of a 1 mΩ resistor be contributing to the SOC jumps I’m seeing during rest?

Best regards,

Etienne Mandeville