This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27Z558: Setting Inquiry for learning cycle

Part Number: BQ27Z558

Tool/software:

Hi, team.

I would appreciate if you could help configuring some setting for learning cycle.

1. Design Capacity : 4320 mAh - Nominal capacity of pack(cell)

2. Charge Term Taper Current : 220 mA - During learning cycle, I will stop charging when charging current is about 200mA

  • After learning cycle is completed, I'll use this battery at PDA, and the charge taper current of PDA will be 200mA.

3. Dsg Current Threshold : 60 mA

4. Chg Current Threshold : 75 mA

5. Quit Current : 40 mA

6. Term Voltage : 3000 mV - Dishcharge cut-off voltage is 3000 mV in cell and battery pack datasheet

  • Term Voltage setting will be 3400mV after learning cycle is completed - Term voltage is 3400 mV in PDA(0%)

Thanks,

Jaiyong