Tool/software:
Hi Team,
Please help to review schematic, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Attached is the updated quickstart calculator with the updated external compensation BOM. One thing to note is the input and output ceramic capacitors. Ceramic capacitors have capacitance derating when voltage is applied to them. Therefore, when capacitance values are entered in the calculator, it is the capacitance derating value that needs to be used. You can fine most of these values on the component's website such as Murata and TDK. See link for example of output capacitors if Murata capacitors are used:
LM704A0_quickstart_calculator_A1_06092025.xlsm
Ben